Rated for 300V & 4-6A, the new, one- to four-position 9176-800 Series low-profile IDCs deliver high-reliability performance in a wide range of space-constrained, harsh-environment, 22-26AWG industrial, medical, & transportation applications

FOUNTAIN INN, S.C. (April 18, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, has released the new 9176-800 Series low-profile insulation displacement connectors (IDCs), which reduce the Z-axis height of the next-lowest-profile insulated IDC connector, the 9176-400 Series, by 1mm, reduce the total overall volume of the Standard 00-9176 Series IDCs by more than 50%, and are the first industrial IDCs available in a 2.55mm profile.

Designed to connect discrete 22-26AWG solid and stranded wires and leaded components to PCBs, or to connect PCBs together in a daisy chain configuration, the new 9176-800 Series low-profile IDCs are available in a range of sizes extending from one to four positions in each wire gauge, and feature redundant, fatigue-resistant phosphor bronze contacts that provide gas-tight, cold-welded wire connections that are compatible with potting and overmolding encapsulation processes for environmental protection. Rated for 300V, 4-6A, and operating temperatures spanning -40°C to +125°C, the series delivers high-reliability power and signal connections in space-constrained, harsh-environment industrial, medical, and transportation applications including: smart metering, sensors, building controls, portable monitoring and measuring devices, point-of-sale equipment, handheld inventory management devices, security systems, patient monitoring equipment, and LED lighting.

"We developed our new 9176-800 Series low-profile IDCs with an industry-leading 2.55mm profile to provide design engineers working in the industrial, medical, and transportation markets with robust, high-reliability interconnect solutions ideal for use in a wide range of high-density, space-constrained applications exposed to harsh environmental conditions," said Tom Anderson, connector product manager at AVX Interconnect. "AVX leads the market offering of 22-28AWG IDC solutions, and our IDC technology is backed by more than 10 years of proven performance in rugged industrial and transportation applications."

The new 9176-800 Series low-profile IDC connectors feature a flat, integral, glass-filled Nylon 46 cap compliant with UL94 V-0 and designed for automated pick-and-place assembly, and enable simple, single-step termination. To further ensure error-free termination, the one-position versions are also available in eight colors designed to match individual wires. Current ratings are reliant upon AWG; the 22AWG connectors are rated for 6A, the 24AWG connectors are rated for 5A, and the 26AWG connectors are rated or 4A, and every connector in the series is rated for three-cycle durability. Parts are packaged in tape and reel in quantities of 1,700, UL approval is expected in April 2018, and 28AWG versions are currently in development.

For more information about AVX's new 9176-800 Series low-profile insulation displacement connectors, please visit http://www.avx.com/products/connectors/wire-to-board/low-profile-idc-22-26awg-9176-800/. For all other inquiries, please visit www.avx.com, email inquiry@avx.com, follow them on LinkedIn and Twitter, like them on Facebook, call 864-967-2150, or write to One AVX Boulevard, Fountain Inn, S.C. 29644.

About AVX

AVX Corporation is a leading international manufacturer and supplier of advanced electronic components and interconnect, sensor, control and antenna solutions with 29 manufacturing facilities in 16 countries around the world. AVX offers a broad range of devices including capacitors, resistors, filters, couplers, sensors, controls, circuit protection devices, connectors and antennas. AVX components can be found in many electronic devices and systems worldwide. The company is publicly traded on the New York Stock Exchange (NYSE:AVX).

For more information, please visit www.avx.com, call 864-967-2150, or write to One AVX Boulevard, Fountain Inn, SC 29644.