Vishay Intertechnology's T59 Series of vPolyTan™ Low-ESR Polymer Capacitors Honored With 2017 ACE Award

MALVERN, Pa. — Dec. 12, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its T59 series of vPolyTan™ multi-anode polymer surface-mount chip capacitors has been recognized with a 2017 ACE (Annual Creativity in Electronics) Award. The awards program, sponsored by EE Times and EDN magazine, recognizes leading companies, products, and people in today's electronics industry. The T59 series was selected as the winner in the category of Passive, Interconnects and Electromechanical.

more ...

Stackpole Releases High Voltage Axial Leaded Resistors

RALEIGH, NC (December 7, 2017) -- Stackpole Electronics, Inc. announces the release of the HVAM series of high voltage axial leaded resistors. The HVAM deposition technology produces a non-inductive resistive element with high stability, low noise and high voltage ratings. Precision tolerances are available down to 0.1% with TCR as low as 50 ppm. Resistance values range from 500 Kohm to 10 Gohm, depending on resistor size and tolerance. Sizes and maximum working voltage ratings are as follows:

more ...



Complete Full-Bridge System-in-Package from STMicroelectronics Includes MOSFETs, Gate Drivers, and Protection to Save Space, Simplify Design, and Streamline Assembly

Geneva, December 4, 2017 -- STMicroelectronics’ PWD13F60 System-in-Package (SiP) contains a complete 600V/8A single-phase MOSFET full bridge in a 13mm x 11mm outline, saving bill-of-materials costs and board space in industrial motor drives, lamp ballasts, power supplies, converters, and inverters. With a footprint 60% smaller than a comparable circuit built from discrete components, the PWD13F60 can also boost end-application power density. By integrating four power MOSFETs, it presents a uniquely efficient alternative to other modules on the market that are typically dual-FET half-bridge or six-FET three-phase devices. Unlike either of these choices, only one PWD13F60 is needed to implement a single-phase full bridge, leaving no internal MOSFETs unused. There is also flexibility to configure the module as one full bridge or two half bridges.

more ...

Pulse Electronics Networking BU Expands 5GBase-T LAN Product Line

Pulse Electronics Networking BU today unveiled its first full product line of 5GBase-T Ethernet Transformers and Connector Modules. We are bringing more package options, extended temperature solutions, and more bandwidth to your applications with a complete range of 5GBase-T Ethernet Transformers and Connector Modules. Samples are available for engineers to now choose between single, 1x1, and 2x4 ports.

more ...

TE Connectivity Partners with Andretti Technologies to Inject Electric and Advanced Tech into Motorsports Engineering

December 7-9, 2017 IS Motorsport & TE Connectivity Booth #3625, Yellow Hall Indiana Convention Center Indianapolis, Indiana. In the world of autosport, milliseconds matter and can be the difference between first and second place. TE supports the Andretti Formula E motorsport team’s engineers and their goal to be the world’s top electric race team. This unique technical partnership between engineers from both organizations drives the future of motorsports and innovation for new clean-energy racing solutions.

more ...

Vishay Intertechnology's T59 Series of vPolyTan™ Low ESR Polymer Capacitors Named as 2017 ACE Awards Finalist

MALVERN, Pa. — Nov. 30, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its T59 series of vPolyTan™ multi-anode polymer surface-mount chip capacitors has been chosen as a 2017 ACE (Annual Creativity in Electronics) Awards finalist. The awards program, sponsored by EE Times and EDN magazine, recognizes "the best of the best in today's electronics industry, including the hottest new products, start-up companies, design teams, executives, and more." In the category of Passive, Interconnects and Electromechanical, the T59 series was selected as one of three finalists.

more ...

New Automation Systems Can Be Smaller, Smooth, and Silent with Advanced Motion-Control Chip from STMicroelectronics

Geneva, November 27, 2017 – The fine motor skills of precision robots can become even more advanced using the latest electronic innovation from STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications. Sophisticated, space-saving advanced laboratory-automation systems are helping medical centers cut clinical costs and accelerate turnaround times - to provide high-quality care for more patients - while industrial robotics including 3D printing have greatly enhanced accuracy and throughput in recent years. 3D printers can produce parts with complex shapes, quickly and accurately, and are becoming more and more affordable, for consumer and professional uses from prototyping to production.

more ...