AVX Releases New High-Performance MLO® Band-Pass Filters For RF/Microwave Applications

FOUNTAIN INN, S.C. (May 3, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, has released a new series of low-profile, high-performance band-pass filters based on AVX's patented and proven multilayer organic (MLO®) high-density interconnect technology. The new BP Series MLO band-pass filters incorporate high-dielectric-constant and low-loss materials that are expansion matched to most organic PCB materials, providing improved reliability over standard silicon and ceramic devices, feature an ultralow profile of less than 0.556mm, and support 18 pass bands spanning 620-5,930MHz. The series also exhibits low insertion loss (1.57-2.41dB typical), low parasitics, 50Ω impedance, excellent rejection of out-of-band frequencies, and favorable heat dissipation characteristics, and is rated for 1W continuous RF power, making it ideal for use in a wide range of wireless applications, including: wireless communications systems, military and emergency first responder radios, UAVs, base stations, femtocells, microcells, wireless access points and terminals, and instrumentation equipment.

more ...

AVX is Sponsoring & Attending EDS 2018

FOUNTAIN INN, S.C. (May 2, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, is sponsoring and attending the 2018 Electronic Distribution Show (EDS), which will take place May 15-18 at the Mirage Hotel and Casino in Las Vegas.

more ...

AVX Earns 2017 TTI Supplier Excellence Award

FOUNTAIN INN, S.C. (April 30, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, has earned a TTI Supplier Excellence Award in the Americas region for the fourth consecutive year. Bestowed by TTI, Inc., an authorized, specialty distributor of interconnect, passive, and electromechanical (IP&E) components, the TTI Supplier Excellence Award recognizes AVX for having successfully fulfilled several key quality performance metrics designed to elevate supplier and distributor performance and achieve maximum customer satisfaction throughout the Americas.

more ...

AVX is Showcasing High-Temperature Capacitor Solutions at HiTEC 2018

FOUNTAIN INN, S.C. (April 27, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, is showcasing its portfolio of high-temperature capacitor solutions during the exposition portion of the International Microelectronics Assembly and Packaging Society's (IMAPS') International Conference on High Temperature Electronics (HiTEC 2018), which will take place May 8-10 in Albuquerque, New Mexico, and is widely recognized as the industry's premier biennial technical conference dedicated to the advancement of high-temperature electronics research and applications.

more ...

AVX Releases the First Industrial Insulation Displacement Connectors With a 2.55mm Profile

FOUNTAIN INN, S.C. (April 18, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, has released the new 9176-800 Series low-profile insulation displacement connectors (IDCs), which reduce the Z-axis height of the next-lowest-profile insulated IDC connector, the 9176-400 Series, by 1mm, reduce the total overall volume of the Standard 00-9176 Series IDCs by more than 50%, and are the first industrial IDCs available in a 2.55mm profile.

more ...

AVX to Present & Exhibit at the 2018 Components for Military & Space Electronics Conference & Exhibition

FOUN & TAIN INN, S.C. (April 16, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, will deliver two technical presentations, teach a tutorial training seminar, co-chair a conference session, and exhibit at the 22nd annual Components for Military & Space Electronics Conference & Exhibition (CMSE 2018), which will take place May 7-10, 2018 at the Sheraton Four Points Hotel in Los Angeles.

more ...

New BTB Pin Jumpers for Maximum Tolerance Absorption in SSL & Industrial Applications

FOUNTAIN INN, S.C. (April 12, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, has released a new series of pin jumpers designed for board-to-board (BTB) and module-to-module connections in solid-state lighting (SSL) and other low-pin-count industrial applications. When used in conjunction with the new 2.5mm 70-9296 Series STRIPT™ horizontal, poke-home contact without a wire stop - which is both the first industrial poke-home connector available without an integral wire stop and, currently, the only industrial poke-home connector with a 2.5mm profile - the new 10-9296 Series BTB pin jumpers are allowed to pass straight through the contacts, completely unrestricted, until the final, user-defined mating dimension is achieved. Unlike traditional BTB pin jumpers - which are made to mate with traditional connectors and are thus closed on the back end, limiting the depth to which a pin can travel and restricting the amount of BTB or module-to-module mating tolerance that the jumper can absorb - the new 10-9296 Series BTB pin jumper/709296001025016 contact combination absorbs the maximum amount of component and assembly tolerances during the mating process, effectively eliminating the PCB and housing tolerance stack-up issues common to traditional connector systems in linear and coplanar applications.

more ...

AVX Releases the First Industrial Poke-Home Connector Available Without a Wire Stop

FOUNTAIN INN, S.C. (April 9, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, has released the first industrial poke-home connector available without a wire stop. The new 2.5mm poke-home contact - the latest addition to its 70-9296 Series STRIPT™ insulator-less, single-position, horizontal, poke-home contacts - combines a low profile with an industry-leading range of compatible wire gauges: 20-26AWG solid and stranded wire, and is the first in the series and on the market to offer variants both with and without a wire stop.

more ...

AVX is Presenting & Exhibiting at APEC 2018

FOUNTAIN INN, S.C. (February 19, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, is presenting and exhibiting at the 2018 Applied Power Electronics Conference (APEC), which will take place at the Henry B. Gonzalez Convention Center in San Antonio, Texas, March 4-8.

more ...

AVX is the First to Offer Space-Level X7R BME MLCCs Approved to MIL-PRF-32535

FOUNTAIN INN, S.C. (February 16, 2018) - AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, is the first - and currently only - company to offer space-level, X7R base metal electrode (BME) MLCCs with "M" and "T" reliability levels approved to the Defense Logistics Agency's (DLA's) MIL-PRF-32535 specification. Exhibiting high CV capabilities superior to those of precious metal electrode (PME) MLCCs, which have long been the standard for the global aerospace industry, AVX's leading-edge, space-level, X7R BME MLCCs deliver a 39-fold increase in capacitance compared to standard, 100V, 1812, MIL-PRF-123 and MIL-PRF-55681 MLCCs - enabling revolutionary board space, weight, and component count reductions that directly translate into lower launch costs - and meet extremely stringent DLA requirements for high-reliability performance in space applications. The series also features AVX's patented FLEXITERM® termination technology, which allows for more board flexure than standard terminations, providing proven-effective protection against thermal and mechanical stresses both during assembly and throughout component lifetimes and enabling the safe, reliable employment of large case sizes.

more ...