Bourns Ultra-Low Capacitance TVS Diode Array for Gb Ethernet Ports

RIVERSIDE, Calif., August 8, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a TVS diode array designed to provide effective surge protection in high-speed communication port and sensitive transceiver applications. The Bourns® Model CDDFN10-2574N TVS diode array features a DFN10 package that uses a flow-through layout to enable minimal impedance change, which is a critical requirement for high-speed ports such as Gigabit Ethernet (GbE). Furthermore, its ultra-low capacitance of only 1.7 picofarads minimizes signal degradation on each channel.

more ...


Analog Devices Expands GaN Power Amplifier Portfolio with Two Broadband 6-GHz Modules

Analog Devices, Inc. today announced a pair of high-performance gallium nitride (GaN) power amplifier (PA) modules which offer one of the highest power-density levels in their class, thus minimizing size and weight of the subsystem. The HMC7885 and HMC7748 broadband modules target applications operating between 2 GHz and 6 GHz, including test and measurement, communications, Traveling Wave Tube (TWT) replacement, military/aerospace surveillance and countermeasures, and radar. The fully integrated, all solid-state devices expand ADI's existing line of GaN-based PAs, and feature ease of use to accelerate prototyping and system design.

more ...

TE Connectivity Displays Rugged Fiber Optics for Defense Systems at 2016 AUSA

Members of the media are invited to visit TE Connectivity (TE), a world leader in connectivity and sensors, at booth #8123 at the 2016 AUSA Annual Meeting and Exposition. TE will display its many advanced fiber optic products and high-speed end-to-end solutions for military and defense applications like weapons systems, vetronics, communications and power distribution.

more ...