Medical-Oriented System Brings a Sense of Peace and Comfort

MD711-SU is a medical computing system designed to facilitate clinical environments, enhance high efficiency and safety during treatment, and reduce diagnostic errors in healthcare solutions. Completed with easy-to-use universal I/O interface and anti-bacterial design, clinicians are free to adapt this medical grade computer in hygienic environments. It also has the most silent fanless design built in solution among other medical computers and can be used in noise-sensitive environments. At the forefront of medical computer with user-friendly smooth surface and long-term support, it makes a dedication to various healthcare applications.

more ...



DFI, Now With Qidsa - a Top 100 Global Tech Leader, Serves You Better than Ever

To strengthen our competence and provide customers with higher added values, DFI has joined Qisda/BenQ Group at the end of 2017 to take technology, supply chain management, and manufacturing productivity to a new level. By leveraging diversified resources within Qisda/BenQ Group, we’re offering more extensive embedded computing products with advanced services that cover LCD in-house integration, PCB & system assembling, measurement lab, and enclosure capability. Furthermore, we provide flexible small volume with high variety to large scale and cost-efficient production. And more comprehensive solutions including factory automation, digital healthcare, smart energy, and IoT related applications for your future business.

more ...

DFI Update of Intel Security Vulnerabilities Issue

DFI is aware of the new side-channel analysis vulnerabilities (also known as Meltdown and Spectre), which may allow an attacker to gain unauthorized disclosure of information and obtain sensitive data. We recommend our customers to adopt OS & BIOS updates for malware protection. DFI will release the updates that address these vulnerabilities and continue to closely work with Intel to investigate and mitigate any potential impact to affected products and will update this article frequently.

more ...

Learn How DFI’s Highly Reliable and Long Life IPC fitting to Your Industries

When system integrators are trying to find an embedded computer for the equipment, which needs to operate in a critical factory environment, there are several must-have features to ensure the production is efficient and stable 24/7. These features include rugged enclosure design, reliable non-stop operation, long product life cycle support, endurance in harsh conditions, and exceptional processing capability. Tailored to the application, DFI’s EC800-AL fanless industrial computer is equipped with new generation Intel Atom® Processor E3900 series and highly rugged system structure suitable for the variable requirements of industrial control and automated inspection on the shop floor.

more ...


Increase Rugged and Reliability to Your IoT Gateways

DFI’s EC800-AL embedded system is powered by the energy-efficient Intel Atom® Processor E3900 tailored to IoT gateways with the recent increasing demand. It’s a new member of DFI’s compact system product line series. This new model keeps the fanless design in an ultra-small size, supporting 15-years long life cycle while providing enhanced computing, graphics performance, and expandability when compared to the former generation.

more ...

The Most Powerful Boards DFI Ever Had With Intel® Xeon® Processor Scalable Family

Today DFI announced its newest development in industrial motherboard with the groundbreaking Intel®Xeon® Processor family (Purley). It can fit into demands that require heavy business workloads with high agility, reliability, and security. Intel claims the new processor family is the “biggest platform advancement”, and it supports brand-new memory architecture and accelerat es technology. This powerful platform marks the next level of industrial computer, bringing out unparalleled performance and increased computing capability at extremely low latencies while providing improved reliability and high-throughput data communication.

more ...

Ultra-Speed Data Transmission Boosts Up Your Server-Oriented Applications

The amount of data transmission on the Internet is rapidly increasing, resulting from the expansion of cloud computing. As the driving force of server equipment, embedded modules play an important role in processing and transmitting these massive data. However, the specifications and standards of the current modules are mostly for industrial purposes rather than server oriented design. The international organization “PICMG” defines that the standard “COM Express Type 7” should tailor to server-type module to fulfill the requirements of network intensive implementations.

more ...