Military & Defense Solutions Enhance Survivability on the Connected Battlefield

Members of the media are invited to visit TE Connectivity (TE), a world leader in connectivity and sensors, at the 2017 AUSA Annual Meeting and Exposition to witness the launch of its line of O.C.H. micro circular connectors authorized for use in the U.S. Army’s Nett Warrior Soldier vests and peripheral devices. In addition, attending members of the media will have the opportunity to explore TE’s wide range of other military and defense solutions. The Nett Warrior program was developed to meet the need for instant situational awareness and communications capabilities that the modern battlefield demands. TE’s O.C.H. micro circular connectors enable Nett Warrior systems to provide dismounted Soldiers with this connectivity without increasing weight or sacrificing performance.

more ...

Stackpole's MELF Resistors are AEC-Q200 Qualified for Harsh Environments

RALEIGH, NC (September 13, 2017) -- Stackpole has recently introduced the MLFA Series of metal film melf resistors. The MLFA Series is fully AEC-Q200 compliant and offered in the 0204 (0.4W) and 0207 (1W) sizes. The MLFA has exceptional stability demonstrated over life, biased humidity, and short time overload testing. In addition, the MLFA offers pulse power handling up to 3500 watts for single short duration pulses, and lightning surge withstanding up to 6KV for resistance values above 100K ohms. This outstanding performance is ideal for applications including industrial / outdoor controls, electric and fuel powered engine controls, power control and monitoring, automotive applications, and telecom infrastructure.

more ...

TE Connectivity’s Nex-Gen Composite Connectors Provide Rugged Reliability in Harsh Environments

TE Connectivity (TE) (NYSE: TEL), a world leader in connectivity and sensors, has released its next generation ACT composite connectors within the DEUTSCH MIL-DTL-38999 series. The ACT series circular connectors are among the most versatile and popular circular mil spec input/output connectors in the world. These circular connectors offer composite shells providing up to 40 percent weight savings over aluminum connectors.

more ...

TE Connectivity’s Next Generation Composite Connectors Provide Rugged Reliability in Harsh Environments

TE Connectivity (TE) (NYSE: TEL), a world leader in connectivity and sensors, has released its next generation ACT composite connectors within the DEUTSCH MIL-DTL-38999 series. The ACT series circular connectors are among the most versatile and popular circular mil spec input/output connectors in the world. These circular connectors offer composite shells providing up to 40 percent weight savings over aluminum connectors.

more ...