HDM Series Economical Axial Leaded Resistors Offer Anti-Moisture Performance and 1% Tolerance

RALEIGH, NC (Mar. 28, 2018) – The HDM series from Stackpole is an axial leaded carbon film technology resistor with outstanding moisture withstanding capability. Axial leaded resistors that need to withstand high humidity typically require a metal glaze technology which is considerably more expensive. The HDM series can survive 100 hours in a pressure cooker at 120ºC, over 98% relative humidity and 2 atmosphere’s pressure while standard carbon film and metal film resistors would fail.

more ...

High Voltage Precision Chip Resistors from Stackpole

RALEIGH, NC (March 22, 2018) -- The HVC series from Stackpole is a thick film surface mount chip resistor series designed for high voltage handling and high resistance values. The HVC has low VCR, TCR available down to 25 ppm, and tolerances as low as 0.1%. Voltage ratings for the HVC are as follows:

more ...

Stackpole Thin Film Resistors AEC-Q200 Compliant Available in 0.01% Tolerance and 2ppm TCR

RALEIGH, NC (Jan. 24, 2018) – Stackpole’s RNCF is an AEC-Q200 compliant series of precision thin film chip resistors. The RNCF offers sizes from 0201 up to 2512, with a tolerance of 0.01% and TCR of 2 ppm available for a select value range for sizes from 0402 through 2512. This exceptional performance makes the RNCF ideal for precision applications such as instrumentation, medical applications and monitoring, precision controls, avionics, telecom, industrial controls, as well as test and measurement equipment.

more ...

Amphenol RF Introduces Line of Fixed Length SMPM Cable Assemblies

Amphenol RF introduces fixed length SMPM cable assemblies as the ideal pre-configured solution for high frequency applications with 50 Ohm impedance requirements. The cable assemblies offer excellent performance up to 20 GHz and are designed for high reliability requirements including military and aerospace applications.

more ...

RNCF Series Precision Thin Film Chip Resistor

Stackpole recently expanded the resistance value ranges of the 0201 chip size of the RNCF Series of precision thin film chip resistors. Resistance values from 49.9 ohm to 33K ohm are now available in tolerances as tight as 0.5% and TCR as low as 25 ppm. With the proliferation of consumer electronics and the desire for smaller, lighter and more portable devices, the 0201 chip size is often necessary. This expansion allows for increased precision for electronics such as instrumentation, test equipment, precision controls, diagnostic equipment, and medical electronics.

more ...

Stackpole Expands Small Size Precision Chip Resistor Values

The RNCF Series from Stackpole is a precision thin film chip resistor series capable of achieving tolerances as tight as 0.01% and TCR as low as 2 ppm/ºC. Stackpole recently expanded the resistance value range for the 0402 chip size for all tolerances to offer values from 49.9Ω up to 20KΩ.

more ...

AVX Releases New Multilayer Organic High Pass Filters for Wireless Applications

AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has released a new series of low profile, high pass filters with best-in-class performance. Based on AVX's patented and proven multilayer organic (MLO®) high density interconnect technology, the new HF Series MLO high pass filters utilize high dielectric constant and low loss materials to help engineers integrate high Q passive printed elements, such as inductors and capacitors, in multilayer stacks with land grid array surface mount packaging that's expansion-matched to most organic printed circuit board materials, providing improved reliability over standard silicon and ceramic devices.

more ...

Stackpole Introduces the RTAN Series Precision Thin Film Tantalum Nitride Chip Resistors

Stackpole Electronics, Inc. announces the release of their new RTAN series chip resistors. The AEC qualified RTAN is a Tantalum Nitride precision thin film resistor that is impervious to moisture corrosion. This type of thin film technology passes biased humidity testing at 85°C, 85% relative humidity, and 10% rated power for more than 1000 hours with very little shift in resistance. In addition, the materials and design are such that the RTAN is resistant to sulfur contamination and will pass the industry standard sulfur test ASTM B809-65 with minimal resistance shift.

more ...

Stackpole's MELF Resistors Offer Lower Thermal Resistance

Stackpole's MLF / MLFM is a series of metal film, surface mount MELF resistors. The MELF technology provides cooler operating temperatures than flat chip resistors at full rated power. For example, the MLFM1 will typically run more than 70°C cooler than the equivalent 1W 2512 size flat chip resistor and has a smaller footprint. The cool operating performance is possible due to the cylindrical shape and solderable end caps of the MLF / MLFM.

more ...

AVX Releases New Multilayer Organic Low Pass Filters With Best-In-Class Performance

AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has released a new series of low profile, low pass filters with best-in-class performance. Based on AVX's patented and proven multilayer organic (MLO®) high density interconnect technology, the new LP Series MLO low pass filters utilize a combination of high dielectric constant and low-loss materials to enable the fabrication of multilayer, stacked passive devices, such as inductors and capacitors, with high volumetric efficiency, high Q, and exceptional electrical performance. Designed to support both a wide frequency range (0.4GHz - 6.5GHz) and several wireless standards, LP Series low pass filters feature an ultralow 0.55mm height profile, and exhibit excellent isolation, low insertion loss (≤1.3dB), low parasitics, and 50Ω impedance, making them ideal for use in a variety of wireless applications, including: mobile communication devices, global positioning systems (GPS), vehicle location systems, wireless LANs, satellite receivers, and instrumentation.

more ...