Vishay Intertechnology Introduces Industry's First IHLP® Inductor Series Qualified to MIL-STD-981 Class S for Space-Grade Applications

MALVERN, Pa. — April 25, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of low profile, high current IHLP® inductors that are the industry's first to meet the requirements of MIL-STD-981 class S. Designed to provide high reliability in space-grade applications, inductors in the Vishay Custom Magnetics SGIHLP series feature a ruggedized package and perform at high operating temperatures to +180 °C.

more ...

AVX Releases New Accu-L® Series Thin Film Chip Inductors for Automotive Signal & Power Applications

FOUNTAIN INN, S.C. (January 22, 2018) -AVX Corporation, a leading manufacturer and supplier of passive components, interconnects, sensors, and control solutions, has released a new series of thin film multilayer chip inductors especially designed to meet demanding performance specifications in automotive signal and power applications. Qualified to AEC-Q200, the new automotive grade Accu-L® Series inductors exhibit ultra-tight inductance tolerances down to ±0.05nH, in addition to: RF power capabilities, high Q, high self-resonant frequency (SRF), low DC resistance (Rdc), and outstanding high-frequency performance from 450MHz to 2,400MHz. Available in small, ruggedly constructed, low profile 0402 and 0805 chip sizes, the series also delivers exceptional intra-lot and lot-to-lot physical and electrical consistency that makes it ideal for use in automotive signal and power applications that require apex accuracy, including: matching networks and filters in vehicle-to-vehicle communications, infotainment, vehicle location, keyless entry, global positioning, and radar systems.

more ...

Bourns Expands Successful Line of Multifuse® Ultra-Low Resistance Surface Mount PPTC Resettable Fuses

RIVERSIDE, Calif., July 18, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has expanded its successful line of ultra-low resistance Multifuse® Polymer Positive Temperature Coefficient (PPTC) resettable fuses. Bourns is introducing the new model series MF-PSML (0805 size) while adding new low-profile devices to the company's existing MF-NSML (1206 size) and MF-USML (1210 size) series products. Bourns is extensively increasing its Multifuse® product line to provide design engineers with a breadth of low-resistance overcurrent and thermal circuit protection solutions that meet their space-constrained application requirements.

more ...

New Vishay Intertechnology IHLP® Inductor Offers High Temperature Performance for Commercial and Industrial Applications in Extreme Environments

Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new IHLP® low profile, high current inductor in the 1616 case size that combines a high operating temperature to +155 °C with a low profile of 2 mm for commercial and industrial applications in extreme environments. With a frequency range up to 2 MHz, the Vishay Dale IHLP-1616BZ-51 is optimized for energy storage in DC/DC converters and high current filtering up to the self-resonant frequency (SRF) of the inductor (see table below). Applications include notebooks, desktop PCs, and servers; low profile, high current power supplies, PMICs, and point of load (POL) converters; industrial and telecommunications power systems; and DC/DC converters for distributed power systems and FPGAs.

more ...

AVX Releases New MS Series MOS Capacitors for DC-20GHz Operation

AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has released new MS Series metal oxide semiconductor (MOS) capacitors for applications in the RF, microwave, and gigahertz ranges. Designed for DC to 20GHz operation in hybrid circuits, bias networks, receiver optical subassemblies (ROSA), transmission optical subassemblies (TOSA), and aerospace and test and measurement equipment, MS Series MOS single-layer capacitors use silicon dioxide (SiO2) dielectric materials to deliver small, low-profile, temperature-stable solutions with high Q, high breakdown voltage, and low leakage. The series also offers a wide capacitance range (1 - 1,000pF), tight capacitance tolerances down to ±0.1pF, and rugged construction.

more ...

Vishay Intertechnology to Showcase Automotive Product Line at SIAT 2017

Vishay Intertechnology, Inc. (NYSE: VSH) today announced its product lineup for the Symposium on International Automotive Technology (SIAT) 2017, which takes place Jan. 18-21 at the ARAI Campus in Pune, India. Exhibiting in booth 159 with a "Think Automotive, Think Vishay" theme, Vishay will highlight a wide range of products from its automotive product line, including capacitors, resistors, inductors, diodes, MOSFETs, and optoelectronics designed to meet and exceed AEC qualifications.

more ...

Vishay Intertechnology Releases Commercial Version of the Popular Automotive Grade IHLE Integrated E-Shield Inductor

Vishay Intertechnology, Inc. (NYSE: VSH) today announced a commercial version of its popular Automotive Grade IHLE series of low profile, high current inductors featuring integrated e-shields for EMI reduction. Available in the 2525, 3232, and 4040 case sizes, the Vishay Dale IHLE-2525CD-51, IHLE-3232DD-51, and IHLE-4040DD-51 contain the electric field associated with EMI in a tin-plated copper integrated shield, providing up to -20 dB of electric field reduction at 1 cm (above the center of the inductor) when the integrated shield is connected to ground. By eliminating the need for expensive board-level Faraday shielding to lower EMI, the devices reduce costs and save board space.

more ...



Harting DIN 41 612 Type H15 Female Connectors with Press-in Pins

HARTING offers a wide range of standard connectors complying with DIN 41612 and IEC 60 603-2, as well as a great selection of supplementary types and customer specific solutions. Depending on the application, the 3 to 160 way connectors are offered with various termination methods, each contact capable of carrying from 2A to 40A.

more ...