CSRF Foil on Ceramic Current Sense Chip Resistors Offer Low Values in Small Sizes

RALEIGH, NC (Feb. 14, 2018) – The CSRF series from Stackpole is a foil on ceramic carrier technology which offers very low resistance values and low TCR in small chip sizes. With 0.25W rated 0402 size chips in values down to 3 milliohm and 0.5W rated 0603 size chips in values down to 2.5 milliohm, the CSRF is an ideal choice for cutting edge electronics. The consumer electronics industry is pushing more function and content into smaller portable devices and the CSRF is a key addition to the power and battery monitoring and control of the these portable electronic gadgets. In addition the CSRF offers TCR as low as 50 ppm for some sizes and values and tolerances as low as 1% for excellent precision and accurate sensing.

more ...

See the latest connectivity solutions to deliver safer, more efficient connected aircraft

Members of the media are invited to visit TE Connectivity (TE), a world leader in connectivity and sensors, at the 2017 Dubai Airshow to discover how TE is enabling the next generation of connected aircraft to be safer and more efficient. As commercial aircraft become more connected than ever, TE is focused on developing connectivity technologies that reduce size and weight while meeting the demands for higher bandwidths and increased data transfer rates. Designed to perform reliably in the harsh environments of modern aircraft, these technologies are used to control and manage communications and on-board computers for navigation, power management, and multiple subsystems throughout the aircraft.

more ...

STMicroelectronics Combines Unique Development Ecosystem with Alibaba AliOS for First Chinese Cloud-to-Node IoT Platform

Hangzhou, China, October 13, 2017 – STMicroelectronics (NYSE:STM), a global semiconductor leader serving customers across the spectrum of electronics applications, announced today its cooperation with Alibaba Cloud, the cloud computing arm and business unit of Alibaba Group (NYSE: BABA), to provide a complete cloud-to-node IoT solution to the market. The cooperation will allow any designer to easily create IoT nodes and gateways using ST’s key semiconductor building blocks for the IoT, run Alibaba’s IoT operating system AliOS on the node, and seamlessly connect with the Alibaba Cloud for faster time-to-market of large-volume IoT applications.

more ...

Military & Defense Solutions Enhance Survivability on the Connected Battlefield

Members of the media are invited to visit TE Connectivity (TE), a world leader in connectivity and sensors, at the 2017 AUSA Annual Meeting and Exposition to witness the launch of its line of O.C.H. micro circular connectors authorized for use in the U.S. Army’s Nett Warrior Soldier vests and peripheral devices. In addition, attending members of the media will have the opportunity to explore TE’s wide range of other military and defense solutions. The Nett Warrior program was developed to meet the need for instant situational awareness and communications capabilities that the modern battlefield demands. TE’s O.C.H. micro circular connectors enable Nett Warrior systems to provide dismounted Soldiers with this connectivity without increasing weight or sacrificing performance.

more ...