New Vishay Intertechnology Rotational Absolute Magnetic Encoder Displacement Sensor: Higher Durability, Reliability Over Hall Effect Potentiometers

MALVERN, Pa. — Aug. 9, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new magnetic position sensor that delivers accuracy comparable to Hall effect devices while offering higher reliability and better durability. The one-time programmable (OTP) Vishay Sfernice RAME027 provides accuracy of ± 0.33 % at 25 °C in a small 27 mm form factor. Typical applications will include military and industrial joysticks, electrical actuators, machine tools, textile manufacturing, milling, and robotics.

more ...

Vishay Intertechnology RF MLCCs Offer Reliability and Design Flexibility With Industry's First Operating Temps to +200 °C in Small Cases

MALVERN, Pa. — Aug. 7, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the industry's first surface-mount multilayer ceramic chip capacitors (MLCCs) for high frequency RF and microwave applications to offer an operating temperature range to +200 °C. For telecom base stations and military communication systems, the Vishay Vitramon VJ HIFREQ HT series provides ultra high Q and low ESR in four compact case sizes.

more ...

AVX Receives Prestigious 2016 Rockwell Collins Platinum Premier Award

AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has received a prestigious 2016 Rockwell Collins Platinum Premier Award, which honors top-performing suppliers for having maintained the highest levels of quality, delivery, and business alignment over the full course of the year, and is the highest recognition a company can achieve through Rockwell Collins' Trusted Supplier Program.

more ...

Analog Devices Adds POWERLINK to its RapID Platform Network Interface for Improved Design Flexibility and Reliability

Analog Devices, Inc. (ADI) today announced it has added POWERLINK, a real-time industrial Ethernet protocol, to the RapID™ Platform Network Interface developed by the company’s Deterministic Ethernet Technology Group (formally Innovasic, Inc.). The complete, pre-tested, pre-certified solution enables system designers to add Industrial Ethernet to an existing product or to a new product in the fastest time and at the lowest cost. With the RapID Platform Network Interface, system designers have the flexibility to embed the RapID Platform into their field device application as a module or completely embed the module’s components into the field device’s circuit card.

more ...

Vishay Intertechnology Three-Phase-Bridge Power Modules Deliver Efficiency and Reliability for Industrial Applications

Vishay Intertechnology, Inc. (NYSE: VSH) today introduced three new series of three-phase-bridge power modules designed to increase efficiency and reliability for heavy-duty industrial-level applications. The Vishay Semiconductors VS-130MT...C, VS-160MT...C, and VS-300MT...C series deliver higher output current, blocking voltage, and surge current than previous-generation solutions while offering improved thermal resistance in the 5-terminal MTC package.

more ...


Vishay Intertechnology's Professional Thin Film MELF Resistors Provide High Stability and Reliability for Precise Current Measurement in Lighting, Industrial, and Automotive Applications

Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has extended its AEC-Q200-qualified Professional Thin Film MELF resistors to tighter tolerance in the low-ohmic range below 1 Ω for the 0204 and 0207 case sizes. In addition to providing a low temperature coefficient, the improved Vishay Beyschlag MMA 0204 and MMB 0207 allow for more precise current measurement in LED lighting, industrial, automotive, and renewable energy applications with high stability and reliability requirements than previous-generation devices.

more ...

Vishay Introduces New Analog Switch Product Families Built on Advanced Silicon Process That Improves Analog Circuit Performance and Reliability

Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it is upgrading several Vishay Siliconix analog switch products to boost device performance and longevity. Replacing aging silicon technology with an advanced process that improves a range of device parameters while ensuring a useful lifetime well into the future, the move signals Vishay's continuing support for its analog switch and multiplexer product lines, which the company pioneered in the 1960s.

more ...

Analog Devices’ Power Conversion Platform Improves Safety, Reliability and Efficiency in Renewable Energy Applications

Analog Devices Inc . (ADI) today announced its fully integrated power conversion platform for next-generation solar power, energy storage, and electric vehicle infrastructure applications. The platform, which includes processing, gate driving, and sensing components, was designed to enable new faster-switching architectures and accommodate increasing safety regulations.

more ...

AVX to Present Four Technical Papers at CMSE 2016

AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has been invited to present four technical presentations and chair a conference session at the 20th annual Components for Military & Space Electronics Conference & Exhibition (CMSE 2016), which will take place March 6-9, 2016 at the Sheraton Four Points Hotel in Los Angeles.

more ...