High Voltage Precision Chip Resistors from Stackpole

RALEIGH, NC (March 22, 2018) -- The HVC series from Stackpole is a thick film surface mount chip resistor series designed for high voltage handling and high resistance values. The HVC has low VCR, TCR available down to 25 ppm, and tolerances as low as 0.1%. Voltage ratings for the HVC are as follows:

more ...

CSRF Foil on Ceramic Current Sense Chip Resistors Offer Low Values in Small Sizes

RALEIGH, NC (Feb. 14, 2018) – The CSRF series from Stackpole is a foil on ceramic carrier technology which offers very low resistance values and low TCR in small chip sizes. With 0.25W rated 0402 size chips in values down to 3 milliohm and 0.5W rated 0603 size chips in values down to 2.5 milliohm, the CSRF is an ideal choice for cutting edge electronics. The consumer electronics industry is pushing more function and content into smaller portable devices and the CSRF is a key addition to the power and battery monitoring and control of the these portable electronic gadgets. In addition the CSRF offers TCR as low as 50 ppm for some sizes and values and tolerances as low as 1% for excellent precision and accurate sensing.

more ...

Stackpole Thin Film Resistors AEC-Q200 Compliant Available in 0.01% Tolerance and 2ppm TCR

RALEIGH, NC (Jan. 24, 2018) – Stackpole’s RNCF is an AEC-Q200 compliant series of precision thin film chip resistors. The RNCF offers sizes from 0201 up to 2512, with a tolerance of 0.01% and TCR of 2 ppm available for a select value range for sizes from 0402 through 2512. This exceptional performance makes the RNCF ideal for precision applications such as instrumentation, medical applications and monitoring, precision controls, avionics, telecom, industrial controls, as well as test and measurement equipment.

more ...

Stackpole Develops Ultra-high Voltage Chip Resistors

RALEIGH, NC (October 3, 2017) – Stackpole Electronics, Inc. announces the release of the UHV series of ultra-high voltage chip resistors. Resistance values from 100Megohm up to 10Gigohm are available in TCR as low as 100 ppm and tolerances as low as 1%. The UHV typically offers untrimmed resistive elements for 10% tolerances and wider which provide the best stability over life testing and extremely low VCR.

more ...

Stackpole's MELF Resistors are AEC-Q200 Qualified for Harsh Environments

RALEIGH, NC (September 13, 2017) -- Stackpole has recently introduced the MLFA Series of metal film melf resistors. The MLFA Series is fully AEC-Q200 compliant and offered in the 0204 (0.4W) and 0207 (1W) sizes. The MLFA has exceptional stability demonstrated over life, biased humidity, and short time overload testing. In addition, the MLFA offers pulse power handling up to 3500 watts for single short duration pulses, and lightning surge withstanding up to 6KV for resistance values above 100K ohms. This outstanding performance is ideal for applications including industrial / outdoor controls, electric and fuel powered engine controls, power control and monitoring, automotive applications, and telecom infrastructure.

more ...

Stackpole's Precision Chip Resistors Achieve High Resistance

RALEIGH, NC (June 13, 2017) -- The HGC Series from Stackpole utilizes high resistance materials and special patterning to achieve high resistance values with the capability of providing tight tolerances and low TCR. The HGC offers resistance values from 10K ohm up to 50G ohm.

more ...

Stackpole Expands Small Size Precision Chip Resistor Values

The RNCF Series from Stackpole is a precision thin film chip resistor series capable of achieving tolerances as tight as 0.01% and TCR as low as 2 ppm/ºC. Stackpole recently expanded the resistance value range for the 0402 chip size for all tolerances to offer values from 49.9Ω up to 20KΩ.

more ...

Vishay Intertechnology Ultra-Precision Thin Film Chip Resistor Delivers Extremely Low TCR of ± 2 ppm/°C and Tolerance of ± 0.01 in Five Case Sizes

Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new ultra-precision thin film chip resistor that offers a dramatic improvement in TCR and tolerance over previous-generation devices. Available in five case sizes from 0603 to 2512, the Vishay Dale Thin Film PLTU offers a tight TCR of ± 2 ppm/°C and tolerance of ± 0.01 % for industrial, medical, military, and aerospace applications.

more ...

HCC - High Current Chassis Mount Shunt Resistor

Stackpole’s HCC8420 is rated at 15W and has a resistance value of 0.1 milliohm. The HCC8420 has a TCR of 100 ppm/ºC and can handle currents up to 350 amps in a package size measuring 84mm long by 20mm wide. Custom configurations to the value and sensing tabs may be available. Please contact the factory with your specific requirements. The HCC’s high current performance is a good choice for frequency converters, power modules, and battery management for hybrid power sources.

more ...

SM - Surface Mount - General Purpose and Precision Wirewound Resistor

Stackpole Electronics, Inc. has expanded the resistance value range for its SM4527, the 2W surface mount molded wirewound. Resistance values were limited to 0.01 ohm to 0.05 ohms, but now, the robust SM4527 offers values up 1K ohms in tolerances of 1% and 5%. This expansion allows for this popular size to be used for a wider range of applications that require a 2W surface mount resistor with the robust electrical performance and excellent TCR that wirewound technology provides.

more ...