Stackpole Thin Film Resistors AEC-Q200 Compliant Available in 0.01% Tolerance and 2ppm TCR

RALEIGH, NC (Jan. 24, 2018) – Stackpole’s RNCF is an AEC-Q200 compliant series of precision thin film chip resistors. The RNCF offers sizes from 0201 up to 2512, with a tolerance of 0.01% and TCR of 2 ppm available for a select value range for sizes from 0402 through 2512. This exceptional performance makes the RNCF ideal for precision applications such as instrumentation, medical applications and monitoring, precision controls, avionics, telecom, industrial controls, as well as test and measurement equipment.

more ...

Vishay Intertechnology's T59 Series of vPolyTan™ Low ESR Polymer Capacitors Among 2017 ECN IMPACT Award Winners

MALVERN, Pa. — Nov. 20, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its T59 series of vPolyTan™ multi-anode polymer surface-mount chip capacitors was among the winners of the 2017 ECN IMPACT Awards. The awards program, sponsored by ECN Magazine, recognizes the top products and services across 18 categories spanning the design and engineering landscape. In the category of "Passive Components & Discrete Semiconductors," Vishay's T59 series was selected as a winner for the increased volumetric efficiency it provides for computing, telecom, and industrial applications, which reduces component count, saves PCB space, and lowers overall solution costs.

more ...

Bourns Adds New High-Temperature PPTC Resettable Fuses to its Multifuse Line

RIVERSIDE, Calif., July 19, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has added new AEC-Q200 certified high-temperature Polymer Positive Temperature Coefficient (PPTC) resettable fuses to its successful line of Multifuse® products. Offered in 1206 and 1210 (3014 and 3024 metric) surface mount packages and featuring operating temperatures up to 125 °C, Bourns designed the miniature sized MF-NSHT and MF-USHT series as ideal circuit protection solutions for automotive systems, and to provide superior resettable fault protection for a new generation of high density boards in industrial, telecom and consumer electronics that also must operate in elevated temperatures.

more ...


Murata Power Solutions Announces : Murata adds 90A, PMBus™ compliant PoLs for FPGA & processor power

Murata further expands its OKD series of Digital PoL DC-DC converters by launching the 90A/162W OKDx-T/90 series from Murata Power Solutions. This is the highest current-rated product in the OKD series, which already provides solutions from 6A to 60A. The OKDx-T/90 series is ideally suited for FPGA & processor applications. The module is specified to operate over a Vin range of 7.5V to 14V and provides a user-adjustable Vout in the range of 0.6V to 1.8Vdc with industry leading efficiency of 94%. The OKDx-T/90 is available in three different package configurations:

more ...

Fourth-Gen 600 V E Series Power MOSFET Lowers Conduction and Switching Losses, Increases Efficiency

Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the first device in its fourth generation of 600 V E Series power MOSFETs. Providing high efficiency for telecom, industrial, and enterprise power supply applications, the Vishay Siliconix n-channel SiHP065N60E slashes on-resistance by 30 % compared with previous 600 V E Series MOSFETs while delivering 44 % lower gate charge. This results in the industry's lowest gate charge times on-resistance, a key figure of merit (FOM) for 600 V MOSFETs used in power conversion applications.

more ...

AVX Releases A New Series of COTS Plus Polymer Solid Electrolytic Multianode Chip Capacitors

AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released the new high-reliability TCS Series COTS Plus polymer solid electrolytic multianode chip capacitors. Designed for demanding, long-lifetime DC/DC converter applications in telecommunications, industrial, and avionics electronics, TCS Series capacitors feature a robust design consisting of parallel capacitor segments with conductive polymer electrodes in a single package.

more ...

Vishay Intertechnology vPolyTan™ Low-ESR Polymer Capacitors Increase Volumetric Efficiency to Lower Component Counts

Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of vPolyTan™ multi-anode polymer surface-mount chip capacitors that delivers increased volumetric efficiency for computing, telecom, and industrial applications. Combining polymer tantalum technology with Vishay's patented multi-array packaging (MAP), the T59 series delivers the industry's highest capacitance density while maintaining best-in-class ESR.

more ...


Vishay Intertechnology's New 650 V Fast Body Diode MOSFETs Increase Voltage Headroom for Soft Switching in Industrial, Telecom, and Renewable Energy Applications

Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its portfolio of fast body diode n-channel power MOSFETs with the introduction of new 650 V EF Series devices. Augmenting the company's 600 V offering, the Vishay Siliconix SiHx21N65EF, SiHx28N65EF, and SiHG33N65EF provide additional voltage headroom for industrial, telecom, and renewable energy applications when desired.

more ...