High Voltage Precision Chip Resistors from Stackpole

RALEIGH, NC (March 22, 2018) -- The HVC series from Stackpole is a thick film surface mount chip resistor series designed for high voltage handling and high resistance values. The HVC has low VCR, TCR available down to 25 ppm, and tolerances as low as 0.1%. Voltage ratings for the HVC are as follows:

more ...

Bourns New 24 mm Potentiometer Capable of Up to 1 Million Shaft Revolutions

RIVERSIDE, Calif., February 5, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released a new 24 mm potentiometer designed for use in light industrial applications such as test and measurement, communications, clean energy and select medical and diagnostic equipment. Supporting the long cycle life and high reliability needed for these applications, the Bourns® Model PDF241 potentiometer features various flatted and slotted shaft lengths and a long-life carbon element that is capable of up to 1 million shaft revolutions.

more ...

Stackpole Thin Film Resistors AEC-Q200 Compliant Available in 0.01% Tolerance and 2ppm TCR

RALEIGH, NC (Jan. 24, 2018) – Stackpole’s RNCF is an AEC-Q200 compliant series of precision thin film chip resistors. The RNCF offers sizes from 0201 up to 2512, with a tolerance of 0.01% and TCR of 2 ppm available for a select value range for sizes from 0402 through 2512. This exceptional performance makes the RNCF ideal for precision applications such as instrumentation, medical applications and monitoring, precision controls, avionics, telecom, industrial controls, as well as test and measurement equipment.

more ...

Analog Devices to Receive 2017 IEEE Corporate Innovation Award

Analog Devices, Inc. (ADI) today announced that the company has been honored with the 2017 IEEE Corporate Innovation Award “for sustained innovation and leadership in the development of high-performance data converter technology and products.” This award was established in 1985 to recognize outstanding innovation by organizations across the world, and recipients are honored for their resolve to discover, extend, or complement technological advancements in education, industry, research, and service in IEEE fields of interest.

more ...

Stackpole's MELF Resistors Offer Lower Thermal Resistance

Stackpole's MLF / MLFM is a series of metal film, surface mount MELF resistors. The MELF technology provides cooler operating temperatures than flat chip resistors at full rated power. For example, the MLFM1 will typically run more than 70°C cooler than the equivalent 1W 2512 size flat chip resistor and has a smaller footprint. The cool operating performance is possible due to the cylindrical shape and solderable end caps of the MLF / MLFM.

more ...