STMicroelectronics and USound Deliver First Advanced MEMS Silicon Micro-Speakers

Geneva, Switzerland, and Graz, Austria, January 3, 2018 – STMicroelectronics (NYSE:STM), a global semiconductor leader serving customers across the spectrum of electronics applications, and USound, an innovative and fast-growing audio company, have delivered the first silicon micro-speakers resulting from their technology collaboration announced last year. Engineering samples are now with lead customers, and trade demonstrations will take place during CES® 2018, in Las Vegas.

more ...

Murata Power Solutions Announces : Murata adds 90A, PMBus™ compliant PoLs for FPGA & processor power

Murata further expands its OKD series of Digital PoL DC-DC converters by launching the 90A/162W OKDx-T/90 series from Murata Power Solutions. This is the highest current-rated product in the OKD series, which already provides solutions from 6A to 60A. The OKDx-T/90 series is ideally suited for FPGA & processor applications. The module is specified to operate over a Vin range of 7.5V to 14V and provides a user-adjustable Vout in the range of 0.6V to 1.8Vdc with industry leading efficiency of 94%. The OKDx-T/90 is available in three different package configurations:

more ...