Members of the media are invited to visit TE Connectivity (TE), a world leader in connectivity and sensors, to learn how TE autosport products are powering technologies in racing vehicles and beyond.

Autosport Engineering 2018

January 11-12, 2018, TE Connectivity Booth #E440, Hall 9, National Exhibition Centre (NEC), Birmingham, UK

Corrosion is a critical challenge to autosport performance, where every piece of technology can be the difference between winning and losing. TE has a deep history of engineering innovative solutions that address the harsh environments race teams face.

One unique challenge for TE’s engineers was producing a connector that could withstand the harsh, corrosive environment common to race tracks. Salty water on the surface often breaks down other metallic connectors. But TE’s DEUTSCH ACT composite connector range offers corrosion resistance in a small, lightweight package ideal for extreme race applications.

TE representatives will be available at booth #E440 throughout the show to answer questions and participate in interviews. Learn more about TE’s autosport solutions at TE's Autosport Engineering landing page.

DEUTSCH, TE, TE Connectivity and the TE connectivity logo are trademarks of the TE Connectivity Ltd. family of companies.

TE Connectivity Ltd., is a $13 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 78,000 employees, including more than 7,000 engineers, working alongside customers in nearly 150 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat and Twitter.

DEUTSCH ACT SERIES 38999 COMPOSITE CONNECTORS

TE’s next generation composite connectors provide rugged reliability in harsh environments. The DEUTSCH ACT series MIL-DTL-38999 composite connectors offer up to 40 percent weight savings over aluminum connectors. These connectors operate under extreme conditions. These 38999 connectors are widely used throughout the world in defense and aerospace as well as autosport applications because of their rugged capabilities.

Additional Resources:

TE’s Racing Garage

TE’s Autosport Solutions

To learn more or coordinate an interview, contact Erin Zakin at +1 717 652 0100, x106 or via email at ezakin@madewithmerit.com. Connect with our experts today on DesignSmarterFaster.