Device Features High 37.8 A Continuous Drain Current and On-Resistance Down to 8.4 mΩ in Compact PowerPAK® SC-70 Package

MALVERN, Pa. — April 6, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 30 V n-channel TrenchFET® Gen IV power MOSFET that delivers increased power density and efficiency for mobile devices, consumer electronics, and power supplies. Offered in the ultra compact PowerPAK® SC-70 package, the Vishay Siliconix SiA468DJ provides the industry's lowest on-resistance and highest continuous drain current for 30 V devices in 2 mm by 2 mm plastic packages.

60 % smaller than devices in the PowerPAK 1212, the MOSFET released today is one of the most compact 30 V solutions available for DC/DC conversion and load switching for battery management in devices such as notebook computers, tablets, VR headsets, and DC-DC bricks; H bridges in wireless chargers; and motor drive control for drones.

To reduce conduction loss and increase efficiency in these applications, the SiA468DJ features extremely low on-resistance of 8.4 mΩ at 10 V and 11.4 mΩ at 4.5 V. These values represent a 51 % improvement over previous-generation solutions and a 6 % improvement over the closest competing device. In addition, the MOSFET's low gate charge times on-resistance figure of merit (FOM) is optimized for a diverse range of power conversion topologies.

The SiA468DJ's 37.8 A continuous drain current is 68 % higher than previous-generation devices and 50 % higher than the closest competing solution. This high current rating offers an ample safety margin for applications that encounter high transient current. The MOSFET is 100 % RG-tested, RoHS-compliant, and halogen-free.

Samples and production quantities of the SiA468DJ are available now, with lead times of 13 weeks for large orders. Pricing for U.S. delivery only starts at $0.34 per piece.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

Click here to see the original source.