MALVERN, Pa. — April 12, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has extended the useful life of 500 V devices in its 159 PUL-SI series of snap-in power aluminum capacitors. For solar PV inverters, industrial motor control, and power supplies, the Vishay BCcomponents devices now offer a useful life of 5,000 hours at +105 °C.

Featuring a cylindrical aluminum case with a pressure relief valve, insulated with a blue sleeve, 159 PUL-SI capacitors are available in a variety of case sizes ranging from 22 x 25 mm to 35 x 60 mm. Offering rated voltages from 200 V to 500 V, the devices feature high ripple current to 2.80 A, maximum ESR down to 150 mΩ at 100 Hz, and a maximum operating temperature to +105 °C.

As polarized aluminum electrolytic capacitors with a non-solid electrolyte, the 159 PUL-SI series devices are ideally suited for smoothing, filtering, and energy storage in pulsed power applications. The RoHS-compliant capacitors are also available in a keyed polarity snap-in version.

Samples and production quantities of the 159 PUL-SI series capacitors are available now, with lead times of 12 to 14 weeks. Pricing varies by capacitance, voltage, and volume, and ranges from $1 to $10 per piece.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.