SGIHLP Devices Feature High Operating Temperatures to +180 °C in a Rugged Package

MALVERN, Pa. — April 25, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of low profile, high current IHLP® inductors that are the industry's first to meet the requirements of MIL-STD-981 class S. Designed to provide high reliability in space-grade applications, inductors in the Vishay Custom Magnetics SGIHLP series feature a ruggedized package and perform at high operating temperatures to +180 °C.

Featuring a magnetically shielded construction, the devices released today are optimized for DC/DC converters and high current noise suppression filters in satellites and defense systems. Applications for the inductors include low profile, high current power supplies and point of load (POL) converters; "flight-ready" solar inverters; high current filters; and DC/DC converters in distributed power systems.

Offered in five case sizes, the SGIHLP series features high efficiency with typical DCR from 0.56 mΩ to 240 mΩ and a wide range of inductance values from 0.22 µH to 100 µH. Based on proven IHLP technology, the devices provide rated currents to 100 A and handle high transient current spikes without saturation. The inductors offer excellent inductance and saturation stability over the complete operating temperature range.

For more information about the new inductors and to place orders, contact CustomMags@Vishay.com. Technical datasheets can be found at www.vishay.com by entering SGIHLP in the "Part # / Keyword Search" field.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

Click here to see the original source.